can i use code warrior for software simulation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can i use code warrior for software simulation?

2,802 Views
verilogdeepa
Contributor I

can i use code warrior for software simulation?

Labels (1)
0 Kudos
Reply
4 Replies

2,555 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

The answer depends on the device you are using. Chip simulation is only available for S08 and S12 family devices. ColdFire and Kinetis devices cannot be simulated using CodeWarrior, thus you need a debugging tool (PE Micro, Segger).


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,555 Views
verilogdeepa
Contributor I

can i use it on  dsp controllers?

0 Kudos
Reply

2,555 Views
lunminliang
NXP Employee
NXP Employee

What DSP target are you concerning here?

0 Kudos
Reply

2,555 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

I think it is available, but I am not sure if all DSP targets/families can be simulated.

To be sure please repost your question in the DSP forum (CodeWarrior for StarCore) or submit a service request here. In both cases please do not forget to mention the exact number part (unless your question is generic?).

Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply