can i use code warrior for software simulation?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can i use code warrior for software simulation?

2,649 次查看
verilogdeepa
Contributor I

can i use code warrior for software simulation?

标签 (1)
0 项奖励
回复
4 回复数

2,402 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

The answer depends on the device you are using. Chip simulation is only available for S08 and S12 family devices. ColdFire and Kinetis devices cannot be simulated using CodeWarrior, thus you need a debugging tool (PE Micro, Segger).


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,402 次查看
verilogdeepa
Contributor I

can i use it on  dsp controllers?

0 项奖励
回复

2,402 次查看
lunminliang
NXP Employee
NXP Employee

What DSP target are you concerning here?

0 项奖励
回复

2,402 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

I think it is available, but I am not sure if all DSP targets/families can be simulated.

To be sure please repost your question in the DSP forum (CodeWarrior for StarCore) or submit a service request here. In both cases please do not forget to mention the exact number part (unless your question is generic?).

Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复