Write data in the Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Write data in the Flash

1,971 Views
vitorgabriel100
Contributor II

Hello,

I'm utilizing MKW24d board. I would like to know how I could do to write a data block in the flash memory? I also would like to know if there is a example that does it?

Thanks

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,864 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hello, Vitor

 

I have to mention that your device is not recommended for new designs by NXP. However, we can provide you flash memory examples, depending on your IDE.

 

  1. If your IDE is MCUXpresso download the SDK examples for your device  https://mcuxpresso.nxp.com/en/welcome then select the Development board. Download the  SDK archive.  Import an SDK example for flash.  If you are unaware of how to import the example then check this video https://www.nxp.com/design/training/importing-and-using-mcuxpresso-sdk-examples:TIP-PART-4-IMPORTING...

 

  1. If you are using IAR of KDS IDE's go to https://www.nxp.com/downloads/en/protocol-stacks/MKW2xD-MCR20A-Connectivity-Software.exe and download the MKW24 connectivity software.


Have a great day,
Diego

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply