Why Ammclib can not work in interrupt program?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why Ammclib can not work in interrupt program?

2,279件の閲覧回数
amosxue
Contributor II

Follow the User's Guide of Ammclib,I have integrated the lib into CW10.&. It works, when I use the lib in main(),but when I use the lib function in interrupt, it does not work.

extern void usrIsr (void)
{
PIT.CHANNEL[0].TFLG.R=0x1; /*Clear PIT0 Interrupt flag*/
..........
f32Angle = FRAC32 (0.5);
GFLIB_SinCos (f32Angle, &pf32Output);
scope1=pf32Output.f32Arg1;

......

}

Why? How to handle the mistake?

2 返答(返信)

2,143件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please specify, which microcontroller you use and could you please share some simple project?

Regards,

Martin

2,143件の閲覧回数
robert_metzerot
Contributor II

Hello,

was there any solution of this problem? I have the same problems too and use MPC5777C.

I tried to multiply in an ISR. If i call for test the function MLIB_Mul(FRAC32(0.185), FRAC32(0.195), F32) an IVOR1-exception occurs.

Then i tried the function  MLIB_Abs() within this ISR. Its result is the same as input (negative sign) - not ok.

In any loop, which is called from the main loop, all this functions works fine.

Can you give support?

Thank you.

0 件の賞賛
返信