Which version of CodeWarrior has support for MSC8157?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which version of CodeWarrior has support for MSC8157?

ソリューションへジャンプ
1,585件の閲覧回数
yavv
Contributor I

Hello.

 

Which version of CodeWarrior has support for MSC8157 DSP's?

 

I downloaded CW 10.7.2, but it has support for PSC9x3x only.

CW 3.2.3 doesn't support MSC8157 too.

 

Where can I find CW suitable for MSC8157 development?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,523件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

User developing for the MSC8157/8 should use CodeWarrior v10.5.0 which can be downloaded from:

CodeWarrior Legacy Downloads|Freescale

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,524件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

User developing for the MSC8157/8 should use CodeWarrior v10.5.0 which can be downloaded from:

CodeWarrior Legacy Downloads|Freescale

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信