Which one of Special Edition CodeWarrior (free) is suitable for working with TWR-KW24D512 and USB-KW24D512 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which one of Special Edition CodeWarrior (free) is suitable for working with TWR-KW24D512 and USB-KW24D512 ?

1,954件の閲覧回数
wbr
Contributor I

Regards.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,886件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Wojtek Branski:

CodeWarrior does not support KW devices. The next thread might be useful:

CodeWarrior MCU V10.5 creat new project for KW24D512,but codewarrior don't support KW series mcu.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,886件の閲覧回数
wbr
Contributor I

Once more,

Is the BeeKit free solution? I didn't find the information on the site.

Regards

WB

0 件の賞賛
返信

1,886件の閲覧回数
wbr
Contributor I

Hello Jorge

I see, by if I use BeeKit, is it matter which CodeVarior version

(basic,etc) I use to compile exported project?

Regards

WB

0 件の賞賛
返信