Where is the swap_demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the swap_demo

1,980件の閲覧回数
schuylerhorky
Contributor I

The application note at http://www.nxp.com/assets/documents/data/en/application-notes/AN4533.pdf references a program flash memory swap demo in the KINETIS512_SC code examples I downloaded from this thread: Where is the KINETIS512_SC.zip located? , but it's missing from the download.

 

The demo is supposed to show how a K60 can write to its own flash memory and then boot off of it, effectively programming itself in-system, without a programmer.

Thanks in advance,

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,578件の閲覧回数
hmyoong
Contributor III

This is a very useful document to understand Kinetis series ARM microcontrollers. Hope NXP can put up another document for LPC series. If you like this idea, please like this post and hopefully NXP would take note of that.

1,578件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

There Rev2 version of KINETIS512_SC was released already.

You can download it here

ARM Cortex-M4|Kinetis K60 100 MHz 32-bit MCUs|NXP|NXP 

pastedImage_2.png

Kinetis 100MHz Rev 2 Example Projects

Have a great day,
Jennie Zhang

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信