Where can I find the latest version of CCS API and CCS Server.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I find the latest version of CCS API and CCS Server.

6,040件の閲覧回数
saqlainraza
Contributor I

Hi Everyone,

 

I want to use CCS API for communicating with CCS Server in order to debug a target using CodeWarrior USB tap. Can someone please tell me that from where can I download the latest available version of these utilities both for Microsoft Windows and Linux hosts.

 

Thanks.

ラベル(1)
タグ(3)
0 件の賞賛
返信
10 返答(返信)

5,397件の閲覧回数
jiantang
Contributor I

I need this document.if you have get,can you send me a copy? qmmt@sina.com.thanks.

0 件の賞賛
返信

5,397件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Jian

Please use Freescale on line support web page.

  - Go to following URL: http://www.freescale.com/TechSupport

  - You will come to a login page.

  - Click on “Create Service Request”.

  - You can submit your request through the web from there.

Or send mail to support@freescale.com.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

0 件の賞賛
返信

5,397件の閲覧回数
jcrigby2015
Contributor I

I need this also for remote debugging a p1010rdb from a linux host.  Is it available for download from some public place?

0 件の賞賛
返信

5,397件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello John

Please use Freescale on line support web page.

  - Go to following URL: http://www.freescale.com/TechSupport

  - You will come to a login page.

  - Click on “Create Service Request”.

  - You can submit your request through the web from there.

Or send mail to support@freescale.com.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

0 件の賞賛
返信

5,397件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

hi

I see the same question in SR#1-3899590816. What is the part number of your MCU or Processor?

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,397件の閲覧回数
saqlainraza
Contributor I

Hi,

Thanks for the response. I would like to debug different CPU's like P4080,  P2020 and T4020 using CCS API, CCS (Code Warrior Connection Server) and Code Warrior USB /GIGA TAP.

I know that it is possible to use CCS API functions like "ccs_open", "ccs_read_mem", "ccs_read_reg" etc to actually connect to CCS and debug a target CPU using Code Warrior Probe. I need to get the latest versions of these utilities.

Your support is highly appreciated.

Thanks.

0 件の賞賛
返信

5,397件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hi

The latest version should be build 426. I have contacted our engineer, and she will send it to you by TransWeb.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,104件の閲覧回数
healy
NXP Employee
NXP Employee

I also want to this utilities to develop a Hawk V3 memory read & write tool, can you sent me 1 copy of it?

 

thank you so much!

0 件の賞賛
返信

5,397件の閲覧回数
saqlainraza
Contributor I

Hi,

I am unable to open this provided link. It says webpage not available.....

Am I missing something ?

0 件の賞賛
返信

5,397件の閲覧回数
saqlainraza
Contributor I

Thanks for the help ! By when this delivery is expected ?

Regards.

0 件の賞賛
返信