When will Freescale upgrade the CW_HC12_v5.1?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

When will Freescale upgrade the CW_HC12_v5.1?

1,744 次查看
daviddai
Contributor I

Hello together,

 

I have several question about CW_HC12_v5.1:

 

1, For the MCU MM912H634, I can only use CW_HC12_v5.1? How about the latest IDE CW10.6, it supports the MM912H634?

 

2, I used the CW_HC12_v5.1_SPECIAL at this moment, how can I get the full version ?

 

3, When I simulate my program with CodeWorrior True-Time Simullator hiwave.exe,  result is different with full Start/Continue(F5) mode and Step over(F10) mode, why?

    With Step over(F10) mode, some MCU rigisters and some variants I changed the value  in my code have no any change in CodeWorrior True-Time Simullator's detect windows, why? As below:

48337_48337.JPGCapture.JPG                       48440_48440.JPGCapture.JPG

 

Finally, I feel CW_HC12_v5.1 is too old to keep pace with the IDE software development, When will Freescale upgrade the CW_HC12_v5.1?

 

Thanks!

 

Best Regards

David Dai

标签 (1)
0 项奖励
回复
3 回复数

1,269 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

regarding to your questions:

1. you are correct MM912H634 is only supported by CW_HC12_v5.1. CW10.6 doesn't support MM912H634. as I know there is no plan for CW10.x supporting HCS12 in the near future release.

if you want, you can propose your requirement as a feature request to support@freescale.com. Freescale support could escalate it.

2. the long term full version is not free. here is the link to order full version

CodeWarrior Suites (Bas, Stand, Pro)|Freescale

3. regarding to the left side picture, i wonder you debug the project in full simulation mode without connecting board. in full simulation mode, not all hardware register can work normal. you need connect a board to make sure register view perform full function work.

regarding to the right side picture, i wonder it is an optimization problem, please cast the related local variable with volatile:

volatile int i=0;

this should fix the problem.

4. CW5.1 is in maintenance mode, Freescale still develops patch for bug fix. here is the document for

How to download a Service Pack / Patch / Update?

can this help you?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,269 次查看
daviddai
Contributor I

Hello Jennie,

Thanks a lot for your answer!

For the question 3,

Actually, I did connect board, I can drive my motor normally.

How to understand "make sure register view perform full function work"?

For the local variable, also I already cast with volatile, as below.

I else can't detect the real-time change at Stepped Over mode.

Capture.JPG

Thanks!

Best Regards

David Dai

0 项奖励
回复

1,269 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

to avoid optimization, volatile is used for local variable.

for global variable, adding the variable name in prm file ENTRIES section can avoid being optimized. for example:

ENTRIES /* keep the following unreferenced variables */

variable_name1 variable_name2

END

can this help you?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复