Version S19 file during build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Version S19 file during build

1,569 Views
vengeful
Contributor II

Hi,

 

Not sure whether this is possible, but is there a way when generating the output ".s19" file to include a version number. Currently it just takes the name of the project, then I have to rename the file and give a version number manually, this can lead to human error.

 

Using Codewarrior IDE version 5.9

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,464 Views
BlackNight
NXP Employee
NXP Employee

You could run a post-build step where you perform that rename with a version number.

You can execute multiple commands (see Executing Multiple Commands as Post-Build Steps in Eclipse | MCU on Eclipse).

Erich

0 Kudos
Reply