Using Flash Programmer Task for Standalone programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using Flash Programmer Task for Standalone programming

Using Flash Programmer Task for Standalone programming

Standalone Programming is widely used when user doesn’t need a debugger for programming in CodeWarrior 10. Thus people only uses elf/s19 file to program target without using project and source files.

There is a very famous article written by Erich Styger regarding using “Flash File to Target” as a standalone programmer for target programming.

https://mcuoneclipse.com/2012/08/02/standalone-flash-programmer/

 

Besides this method, Flash Programmer Task is also good for standalone programming.  As I know some customers prefer to use this method because it can also do checksum, dump flash,etc during programming. I will introduce how to utilize Flash Programmer Task step by step in the following for brainstorming. This article is based on CodeWarrior 10.6.4 and FRDM-K64 board, but the method is same for all Kinetis,HCS08,HCS12Z,etc devices

 

For detail, see attached article and video.

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎05-23-2016 03:12 AM
更新者: