Use performance analysis tool, but got all results 0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use performance analysis tool, but got all results 0?

1,142 Views
peterzheng
Contributor II

Hi,

 

I was trying to run a bareboard project on P4080DS using CodeWarrior. I need to collect data on CPC hit rate, hence I created a customized scenario for performance analysis tool. And I set up the connection accordingly. Here is the steps I follow:

 

(1) Set the configuration as "Start sampling events when I press "go" button".  "Stop sampling events after 10000 samples". For the rest, I just leave as default

 

(2) Start the profile

 

(3) Run the program I want to profile, I set a break point at the start of the program. It will halt at that break point

 

(4) Press go to start sampling events

 

(5) Resume the program I run

 

(6) After the program terminates, press "stop" button to stop sampling events.

 

Then, afterwards, all the events I have included shows 0. Is there anything I did wrong? Can you help me take a look.

These are the events I have selected.

21251_21251.pngscenario.PNG.png

 

Regards,

Peter

Labels (1)
0 Kudos
Reply
0 Replies