Use codewarrior and PEMICRO to burn program for S08DZ60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use codewarrior and PEMICRO to burn program for S08DZ60

1,832件の閲覧回数
964884547
Contributor I

Hi, I am using codewarrior V6.3 on a 32-bit windows 7 computer to program the S08DZ60 chip. The blue PEMICRO Multilink Universal is used, the version is Rev.D. But the following error occurs:
Loading Target ...
Windows NT detected.
P&E Interface detected-Flash Version 1..4
Frequency change to ~178321hz.
Device is 9S08DZ60.
Mode is In-Circuit Debug.
IO registers loaded for MC9S08DZ60 from C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.3\prog\REG\MCU1027.REG
executing BDM_P&E_Multilink_CyclonePro.hwc

done BDM_P&E_Multilink_CyclonePro.hwc

Error: The debugger is currently not able to run
due to loss of contact with hardware.
No Link To Target
——————————————————————————————————
But in another green version of the writer named Rev.C, it can burn successfully. The information is as follows:
Loading Target ...
Windows NT detected.
P&E Interface detected-Flash Version 6.15
Frequency change to ~15805785hz.
Frequency change to ~18042452hz.
Frequency change to ~8874709hz.
Device is 9S08DZ60.
Mode is In-Circuit Debug.
IO registers loaded for MC9S08DZ60 from C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.3\prog\REG\MCU1027.REG
Startup command file does not exist.
executing BDM_P&E_Multilink_CyclonePro.hwc

done BDM_P&E_Multilink_CyclonePro.hwc

Preload command file does not exist.
Frequency change to ~7968750hz.
executing C:\Users\Administrator\Desktop\Project\bin\Project.xpr

!Data:1 <ADDXPR ONLY_ADD_IF_NEW "AD_Trans_Value"
Target Ready
done C:\Users\Administrator\Desktop\Project\bin\Project.xpr

executing C:\Users\Administrator\Desktop\Project\bin\Project.xpr

!Data:1 <ADDXPR ONLY_ADD_IF_NEW "AD_Trans_Value"
MCU Device Selection has been changed.
done C:\Users\Administrator\Desktop\Project\bin\Project.xpr

Postload command file does not exist.
Frequency change to ~17957746hz.
STARTED
RUNNING
——————————————————————————————————
What may cause the Rev.D programmer to not work normally? It may be
Is the reason for "P&E Interface detected-Flash Version 6.15"

0 件の賞賛
返信
1 返信

1,819件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Codewarrior 6.3 is not recommended to use with windows 7, you can have problems with the USB drivers

Would be possible that you test it on code warrior 11?

 

Regards

 

0 件の賞賛
返信