Updating CW MCU 10.x (Eclipse)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Updating CW MCU 10.x (Eclipse)

1,287件の閲覧回数
kecart
Contributor III

When is it necessary to download the Codewarrior MCU 10.5 (Eclipse) updates (like com.freescale.mcu10_5.PEX_update.v1_0_0.zip) vs letting the IDE find updates and install them?  There are currently 9 updates shown on the website CodeWarrior for MCU 10.5 Updates but the IDE finds at least 15 when a new install does Check for Updates.  At least some of the updates are duplicated between the two methods.

ラベル(1)
0 件の賞賛
返信
1 返信

1,124件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

you can use either use update from
http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_10_5

or

on line update from CW IDE

the updates arrangement may different for these two methods but . both of them includes all the available CW10.5 updates

0 件の賞賛
返信