Update for 9S12XF512?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Update for 9S12XF512?

2,782件の閲覧回数
dermotmurphy
Contributor I

I have loaded CodeWarrior Classic for S12X V5.2 which is the version to use for the #9S12XF512.

However, the software does not include the ability to create a project for the 9S12XF512 nor does it have the required files for this MCU in the lib\hc12c\src folder.

Is there an update package for the IDE and Processor Expert?

If not, how do I modify the installation to allow CW to create projects for the XF512?

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,700件の閲覧回数
dermotmurphy
Contributor I

Hi,

Thank you for this.

Will V5.2 be updated for this MCU, or is this MCU not recommended for new designs.

V5.1 seems very buggy (PE crashes, IDE sometimes will not exit and must be closed using Task Manager).

What is the correct order of installing the service packs?

Thanks

Dermot

0 件の賞賛
返信

2,700件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Dermot

No plan to update CW5.2 for this MCU. This is a marketing decision

I suggest user install compiler patch first then in stall device service pack, then processor expert patch.

0 件の賞賛
返信

2,700件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI Dermot

CW5.2 doesn't support 9S12XF512. please use CW5.1 instead. processor expert support is also included.

Attached is instruction of how to download CW5.1.

Have a nice day,

Jun Zhang

0 件の賞賛
返信