Unable to find the CodeWarrior Debugger Engine executable.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to find the CodeWarrior Debugger Engine executable.

ソリューションへジャンプ
3,042件の閲覧回数
carlesricart
Contributor I

hi,

 

I'm trying to debug with cw10.5 the frdm-K20D50M, but i have errors. When debug, this message error apear: "Unable to find the CodeWarrior Debugger Engine executable."

In the "freescale/ MCU/bin" folder, the DE.exe doesn't appear, and this is weird, if someone can help me...

 

Thanks,

ラベル(1)
0 件の賞賛
返信
1 解決策
2,780件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Carles,

I think your firewall/virus might have removed the DE.exe and moved it into a quarantaine folder. Can you check this?

Probably because the DE.exe wanted to establish a network connection with the debug probe.

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,780件の閲覧回数
carlesricart
Contributor I

Hi Erich,

I desconected the firewall and antivirus and the problem persist.

At first moment, the DE.exe exsist, then when try to debug appears the next error, and then DE.exe disappear.corba error.PNG

Cales,

0 件の賞賛
返信
2,780件の閲覧回数
carlesricart
Contributor I

Erich,

You are correct. The antivirus stopped DE.exe and I didn't see.

Now works. Thank you for all.

Carles

0 件の賞賛
返信
2,780件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Carles,

I think your firewall/virus might have removed the DE.exe and moved it into a quarantaine folder. Can you check this?

Probably because the DE.exe wanted to establish a network connection with the debug probe.

Erich

0 件の賞賛
返信