Unable to connect using PE Micro Universal FX to K60 Tower Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to connect using PE Micro Universal FX to K60 Tower Board

Jump to solution
2,547 Views
Keith4DSmith
Contributor V

I am trying to connect a P&E Micro Universal FX to a TWR-K60F120M running Code Warrior 10.5 under Windows 7.

 

The P&E Micro device has the latest firmware 07.09.

 

I have the latest Jungo USB Multilink 2.0 and WinDriver USB drivers, 11.1.0.0

 

The blue and yellow lights are BOTH on.

 

I have uninstalled the drivers and allowed them to be rediscovered more than once.

 

Below is the log of the debug connection session.

 

I have been able to debug this K60 board using OSJTAG. Now I'm using P&E Micro Multilink FX.

 

What am I doing wrong?

 

=== CodeWarrior GDI protocol log ===

GDI DLL: C:\Freescale\CW MCU v10.5\MCU\bin\Plugins\Debugger\protocols\..\..\support\arm\gdi\arm_pne_gdi.dll

CPU: K60FN1M0

 

 

GDI: DiGdiOpen()

GDI: => DI_OK

GDI: DiGdiGetFeatures()

GDI: => DI_OK

GDI: Identification: ARM Cortex M4 P&E to GDI wrapper, Version: 1.0.1, MeeAvailable: true, NrCpusAvailable: 1

GDI: DiGdiAddCallBack(cb_type = 0x4000)

GDI: => DI_OK

GDI: DiGdiInitIO()

GDI: Mtwks Callback(MTWKS_CB_SETMEEID, 1) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : CWDBG, Entry : LaunchConfiguration, Value : MQX4Equations_RAM_PnE U-MultiLink, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : DO_DEBUG_OUTPUT, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : DEPENDENCY_CHECK, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : UUID, Value : DefaultProject, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : CWDBG, Entry : Processor, Value : K60FN1M0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : ERASE_PROGRAM_WITHOUT_ASKING, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : AUTO_SYNC, Value : 1, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : DOTRIM, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : CURRENT_ALGORITHM_INDEX, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE1_START, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE1_END, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE1_ACTIVE, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE2_START, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE2_END, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE2_ACTIVE, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE3_START, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE3_END, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE3_ACTIVE, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : K60FN1M0, Entry : PRESERVE_EEPROM_START, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : K60FN1M0, Entry : PRESERVE_EEPROM_END, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : K60FN1M0, Entry : PRESERVE_EEPROM, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : ALTERNATIVE_ALGORITHM_PATH, Value : , R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : ALTERNATIVE_ALGORITHM_CHECKBOX, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PARTITION_PARAM, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : DO_PARTITIONING, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : CUSTOM_TRIM, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : K60FN1M0, Entry : TRIM_VALUE, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : NGS_TRIM_OVERRIDE_REFERENCE_FREQUENCY, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : ENABLE_FLASH_PROGRAMMING_DIALOG, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : SPECIFY_NETWORKCARD_ENABLED, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : IO_DELAY_CNT, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP12, Entry : show_hstep_assembly_details, Value : 0, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : CWDBG, Entry : Connect, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : eclipse_show_connection_assistant, Value : 1, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FREQ_FX, Value : 4, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FREQ_NORMAL, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FREQ_OSJTAG, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FREQ_CYCLONE, Value : 3, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FREQ_TRACELINK, Value : 3, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FREQ_LIGHTNING, Value : 1, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FREQ_OPENSDA, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : RESET_DELAY, Value : 100, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : PORT, Value : 21, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : PORT_NAME_STRING, Value : PE5750761, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : interface_selection, Value : 1, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : USE_CYCLONEPRO_RELAYS, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : CyclonePro_poweroffonexit, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : CyclonePro_currentvoltage, Value : 128, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : CyclonePro_PowerDownDelay, Value : 250, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : CyclonePro_PowerUpDelay, Value : 250, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : Multilink_PowerUpDelay, Value : 1000, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : Multilink_PowerDownDelay, Value : 250, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FORCE_MASS_ERASE, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : USE_SWD, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : TraceLink_MaxBufferSize, Value : 1, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : CPUTARGETTYPENAME, Value : , R) => DI_ERR_NONFATAL

INF: P&E Interface detected - Flash Version 7.09

ERR: Can not enter background mode  .

INF: Unable to initialize PEDebug.

GDI: => DI_ERR_NONFATAL

GDI: The Debugger can not connect to the P&E device

GDI: DiGdiClose()

GDI: => DI_OK

Labels (1)
0 Kudos
Reply
1 Solution
2,068 Views
Keith4DSmith
Contributor V

I did move this post to CodeWarrior Development Tools.

I solved my problem.

I had mis-jumpered a peripheral board installed in the tower along with the K60 board.

Once the peripheral board was properly jumpered everything works fine.

Should have been more careful.

View solution in original post

0 Kudos
Reply
2 Replies
2,069 Views
Keith4DSmith
Contributor V

I did move this post to CodeWarrior Development Tools.

I solved my problem.

I had mis-jumpered a peripheral board installed in the tower along with the K60 board.

Once the peripheral board was properly jumpered everything works fine.

Should have been more careful.

0 Kudos
Reply
2,068 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. CodeWarrior Development Tools ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 Kudos
Reply