USB Tap: How attach to a running target, halt it, then load ELF file.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Tap: How attach to a running target, halt it, then load ELF file.

1,784件の閲覧回数
lfa100
Contributor I

I have been looking through the codewarrior documentation, but have not been able to find the steps for doing the following:

1) Attach to a running target.

2) Halt the target

3) Load an ELF file

4) Issue "go" command to start the executable.

 

I have a special boot loaded on the target that sits in a while (1) loop after all initialization is complete (i.e. ram). I would like to perform the listed steps once boot has reached the loop. Maybe this is possible to do via the debugger command shell / command line? It would be nice to avoid the gui as much as possible.

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信