USB Tap: How attach to a running target, halt it, then load ELF file.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB Tap: How attach to a running target, halt it, then load ELF file.

1,785 次查看
lfa100
Contributor I

I have been looking through the codewarrior documentation, but have not been able to find the steps for doing the following:

1) Attach to a running target.

2) Halt the target

3) Load an ELF file

4) Issue "go" command to start the executable.

 

I have a special boot loaded on the target that sits in a while (1) loop after all initialization is complete (i.e. ram). I would like to perform the listed steps once boot has reached the loop. Maybe this is possible to do via the debugger command shell / command line? It would be nice to avoid the gui as much as possible.

 

Thanks

标签 (1)
0 项奖励
回复
1 回复