USB TAP CODE WARRIOR  -DSP56F803 HELP!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB TAP CODE WARRIOR  -DSP56F803 HELP!!

1,227件の閲覧回数
robertyasharzad
Contributor I

Hi,

I have the a.m. item for a wile.  Only using for write and read flash. 

I don't know why - the software disrepair from my computer and I cannot

find it any more. even on the web.

I need it for  DSP56F803.

 

Really appreciated all the good cooperation.

 

Thanks again.

Robert

972-54-3347760

ラベル(1)
0 件の賞賛
返信
1 返信

1,091件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

What tool were you using in your programming?

For DSP56F803 We only have:

1) Classic CodeWarrior v8.3

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC

It supports both USBTAP and parallel, but can only program with ELF file. It works on both Windows XP and Windows 7.  But on Windows 7, user can only use USBTAP for programming, it does not support parallel connection on Windows 7.

2) flash_over_jtag

flash_over_jtag can only support parallel connection, it does not support USB interface.  And it program 56800 with S-record file. It does not support Windows 7 either.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信