USB Multilink versis Tower.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB Multilink versis Tower.

1,294 次查看
dennisdice
Contributor I

@

I am use to using the USB Multilink from P& E.  That is all over now, I have to use the Tower system and make my PC board as big as the tower foot print. If I want to develop with ur micros.

Dennis Dice

标签 (1)
0 项奖励
回复
1 回复

1,178 次查看
trytohelp
NXP Employee
NXP Employee

Hi Dennis,

Most of the time the TWR board includes the OSBDM port and BDM/Jtag post.

By this way you can use the OSBDM (sample UBS cable between the PC and board) or a P&E interface as Multilink Universal.

If you are using CodeWarrior or KDS, the project wizard propose you to select both interfaces.

You will find more details under P&E web site:

    P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...

Hope this will help


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复