USB Multilink Universal Fx Not Showing Hardware Interface Power Control option

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Multilink Universal Fx Not Showing Hardware Interface Power Control option

2,129件の閲覧回数
rampsr
Contributor III

Problem:

My computer I have running CodeWarrior 10.3 does not show the "Hardware Interface Power Control" options when I plug in the USB Multilink Universal Fx. the port shows up as USB1 : Multilink Universal FX Rev A (PE5750211)

141289_141289.PNGmultilinkUniversal_CW103.PNG

 

What update, plugin, or fix is required to make the option available???

 

141290_141290.PNGmultilinkUniversal_CW103_2.PNG

Help!

ラベル(1)
0 件の賞賛
返信
1 返信

2,013件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello rampsr

This feature is added from CW10.3, please see the release note of this update.

To make this option available, please install the update 1.0.0 on your CW10.3. Or upgrade to CW10.6.4:

http://tinyurl.com/6jo5tge

I tested on CW10.6.4, and it also includes this feature, please see the screenshot in below:

screenshot.png

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------