USB Multilink Universal Fx Not Showing Hardware Interface Power Control option

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB Multilink Universal Fx Not Showing Hardware Interface Power Control option

1,211 次查看
rampsr
Contributor III

Problem:

My computer I have running CodeWarrior 10.3 does not show the "Hardware Interface Power Control" options when I plug in the USB Multilink Universal Fx. the port shows up as USB1 : Multilink Universal FX Rev A (PE5750211)

141289_141289.PNGmultilinkUniversal_CW103.PNG

 

What update, plugin, or fix is required to make the option available???

 

141290_141290.PNGmultilinkUniversal_CW103_2.PNG

Help!

标签 (1)
0 项奖励
回复
1 回复

1,095 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello rampsr

This feature is added from CW10.3, please see the release note of this update.

To make this option available, please install the update 1.0.0 on your CW10.3. Or upgrade to CW10.6.4:

http://tinyurl.com/6jo5tge

I tested on CW10.6.4, and it also includes this feature, please see the screenshot in below:

screenshot.png

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------