Trouble when installing the Codewarrior IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trouble when installing the Codewarrior IDE

1,681 Views
xavierbuhot
Contributor II

Hello,

 

I would like to install Codewarrior IDE for HCS08 on my windows 7 64 bit.

 

When I install the IDE I get that error:

"failed to install the inf file ...."

 

 

Can someone have the solution for that problem?

 

Best regard.

Labels (1)
0 Kudos
Reply
2 Replies

1,542 Views
trytohelp
NXP Employee
NXP Employee

Hi Xavier,

as explained Jennie we recommend to use XP OS for MCU V6.3.

This version was not tested under Win 7.

Now there is a problem since Microsoft decided to stop maintenance on XP.

We've already several customers using MCU v6.3 on Win 7.

The installer is not running but a customer found a way to disable the installer OS checking.

A video explaining the process has been posted too.

For more details, please have a look to:

https://community.freescale.com/message/506361

Another solution is to install the tool on XP OS and to copy the installation folder on Win 7 OS.

I've used this solution on my side.

After you must execute the \bin\regserver.bat file.

Hope this will help you.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,542 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hello.

I guess you should install Classic CW(for example CW6.3) on 64bit win7.

CW for HCS08 classic version can't work on 64bit win7. please use CW eclipse v10.6.4 instead.this is our recommendation.

CodeWarrior for Microcontrollers-Eclipse IDE|Freescale

or if you want to use CW6.3 anyway. please refer:

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN3936.pdf?fpsp=1&WT_TYPE=Application Notes&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation&fileExt=.pdf

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply