Toolchain and libraries of CodeWarrior 10.6.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Toolchain and libraries of CodeWarrior 10.6.4

1,898 Views
vigneshbalaji
Senior Contributor I

Hi,

     I want to know the version of Toolchain and libraries that CodeWarrior 10.6.4 is using.

Labels (1)
3 Replies

1,544 Views
ivadorazinova
NXP Employee
NXP Employee

Hi VIGNESH,

Version is 4.7.3

you can find it under C/C++ Build > Build Tool Versions > Version

version.png

I hope this helps.

Best Regards.

Iva

1,544 Views
vigneshbalaji
Senior Contributor I

Thank you Iva,

Now I want to know that if suppose I have a project using 4.7.3 version of GNU Toolchain which CodeWarrior 10.6.4 then if I

move a project Developed in CodeWarrior to KDS 3.0.0 Which uses version 4.8.4 will there be any problem? If so what kind of problems

will occur and how to fix it?

0 Kudos
Reply

1,544 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Vignesh,

you are welcome. Do you have large-size project? If you have small project,is faster to create a new project.

There is created guide for importing project from CW to KDS and there is also described settings for tool chain

CW MCU 10.6 Processor Expert projects migration into KDS 3.0.0

Or you can take a look at the option how to change tool chain in KDS Switching ARM GNU Tool Chain and Libraries in Kinetis Design Studio | MCU on Eclipse

I hope this helps.

Iva

0 Kudos
Reply