Too many projects in a workspace? (CW 10.6)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Too many projects in a workspace? (CW 10.6)

Jump to solution
1,498 Views
chrispawlak
Contributor I

I'm using CodeWarrior 10.6 and I'm wondering if there is a maximum, or a recommended maximum, number of projects for a given workspace. The workspace I'm considering would potentially contain many different projects using various microcontrollers. Would that make CodeWarrior more prone to errors? Would it become too slow? I know CodeWarrior can become slow overtime regardless of the number of projects in a workspace. And I realize you can take care of that by exporting preferences, deleting metadata, and re-importing the preferences. But does it get to a point where it's just always slow because of the high number of projects?

 

Once I decide on a file structure for our code, it will be difficult/confusing to change down the road especially with respect to archiving and version control. So I want to make sure we do it right the first time.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,360 Views
BlackNight
NXP Employee
NXP Employee

Yes, every project open in Eclipse workspace will consume some memory (keeping the symbols, refreshing the files, etc).

So it is best practice to have only the projects open you are working on.

If you are interested in numbers, have a look at

http://mcuoneclipse.com/2014/08/16/eclipse-performance-improvement-tip-close-unused-projects/

Erich

View solution in original post

0 Kudos
Reply
1 Reply
1,361 Views
BlackNight
NXP Employee
NXP Employee

Yes, every project open in Eclipse workspace will consume some memory (keeping the symbols, refreshing the files, etc).

So it is best practice to have only the projects open you are working on.

If you are interested in numbers, have a look at

http://mcuoneclipse.com/2014/08/16/eclipse-performance-improvement-tip-close-unused-projects/

Erich

0 Kudos
Reply