The processor is suddenly grayed out for all the projects!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The processor is suddenly grayed out for all the projects!

Jump to solution
6,356 Views
johnmoore
Contributor I

Last night everything was good so I closed the kinetis IDE and saved my project.  This morning all the projects were red.  So I

reinstalled the CW 10.6 software from a local copy and upgraded it from the help menu.  All projects are still red and the problem

is that the processor component is grayed out.  Mouse hover gives "The component MKL25Z128LK4 is not supported in

this version of processor expert.

 

 

 

 

 

 

Thanks to anyone who knows how to correct this.

 

John

Labels (1)
0 Kudos
Reply
1 Solution
6,185 Views
Rick_Li
NXP Employee
NXP Employee

This issue is a License issue, after shrinking the code size, it works!

View solution in original post

0 Kudos
Reply
9 Replies
6,185 Views
Rick_Li
NXP Employee
NXP Employee

Hi John,

How about to open these projects in a new created workspace?

please let me know the result!

0 Kudos
Reply
6,185 Views
johnmoore
Contributor I

Thanks, Yong Li:

I did create a new workspace and imported projects into it but the result was the same. Red projects.

Then I tried to make a barebones project. Went through all the steps seemingly correctly. But when finished, the wizard did not

create the barebones project in the project explorer!

Thanks,

John

0 Kudos
Reply
6,186 Views
Rick_Li
NXP Employee
NXP Employee

This issue is a License issue, after shrinking the code size, it works!

0 Kudos
Reply
6,185 Views
johnmoore
Contributor I

Yong:

This problem has already been closed, so I

can't check correct answer. You could reopen it and

I'll check the box.

John

---

New Outlook Express and Windows Live Mail replacement - get it here:

http://www.oeclassic.com/

Original Message:

0 Kudos
Reply
6,185 Views
johnmoore
Contributor I

Yong Li:

You and everyone did great in solving this problem. I'm very appreciative.

However there is no place on the discussion now for me to indicate this.

John Moore

---

New Outlook Express and Windows Live Mail replacement - get it here:

http://www.oeclassic.com/

Original Message:

0 Kudos
Reply
6,185 Views
BlackNight
NXP Employee
NXP Employee

Hi John,

if you create a new project with File > New > bareboard project, are the Kinetis devices still listed?

If not, it seems that the Kinetis device support has been uninstalled/removed?

Erich

0 Kudos
Reply
6,185 Views
johnmoore
Contributor I

Erich:

When I created the barebones project, all the devices were properly listed in the wizard.

John

0 Kudos
Reply
6,185 Views
johnmoore
Contributor I

Thanks, Erich:

    I did create a new workspace and imported
projects into it but the result was the same.  Red projects.

    Then I tried to make a barebones project.  Went
through all the steps seemingly correctly.  But when finished, the wizard did
not
create the barebones project in the project explorer!

  

     The software install probably went wrong.  There was a KINETIS error at the end of the software install but no details were available.

Don't know how to add the necessary modules.

     What would be nice is a "repair" installation to correct this kind of problem.  With this, the installer would only replace corrupt or missing files.

Thanks,

John

0 Kudos
Reply
6,185 Views
BlackNight
NXP Employee
NXP Employee

Hi John,

that installation error is very likely the cause of your problems. Can you uninstall it, remove the installation folder from the disk and do a re-install into the default installation folder?

Maybe even your installation image might be corrupted?

Erich

0 Kudos
Reply