The debugging problem of freescale ZVL microcontroller in codewarror10.7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The debugging problem of freescale ZVL microcontroller in codewarror10.7

1,467 次查看
leimengfighting
Contributor I

Dear friend,

Who can help me with the problem?

Can freescale ZVL load ABS files or ELF files for debugging in codewarror10.7 compil?

With best wishes!

Lei

0 项奖励
回复
1 回复

1,412 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello Lei,

Hope you are doing well.

Here is a document using v10.5 but the steps are similar. Please let me know if you have any problems. 

https://community.nxp.com/docs/DOC-329937 

Hope it helps!

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 项奖励
回复