TWR-K70F120M programming trouble

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K70F120M programming trouble

1,523 Views
alexvannewhouse
Contributor II

Howdy,

 

I am pretty new to programming and I have the TWR-K70F120M module. I am trying to start programming but am having trouble learning the system. Does anyone have a simple blink LED code that I can load onto the module, so I can start learning the system.

 

Thanks,

Alex

Labels (1)
0 Kudos
Reply
1 Reply

1,364 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello

- There are sample code in website about this board:

TWR-K70F120M|Tower System Board|Kinetis MCUs|NXP 

pastedImage_2.png

-  Which IDE do you used ?  If CodeWarrior or KDS, you can  also create Processor Expert Project,

it is a great tool for beginner:

pastedImage_1.png

then add the Component, for example if you want to LED project, you can add BitIO or GPIO component,

then there will be Typical Usage:

pastedImage_4.png

I also attached the Processor Expert user guide for you .

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply