TWR-K70F120M programming trouble

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-K70F120M programming trouble

1,538件の閲覧回数
alexvannewhouse
Contributor II

Howdy,

 

I am pretty new to programming and I have the TWR-K70F120M module. I am trying to start programming but am having trouble learning the system. Does anyone have a simple blink LED code that I can load onto the module, so I can start learning the system.

 

Thanks,

Alex

ラベル(1)
0 件の賞賛
返信
1 返信

1,379件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello

- There are sample code in website about this board:

TWR-K70F120M|Tower System Board|Kinetis MCUs|NXP 

pastedImage_2.png

-  Which IDE do you used ?  If CodeWarrior or KDS, you can  also create Processor Expert Project,

it is a great tool for beginner:

pastedImage_1.png

then add the Component, for example if you want to LED project, you can add BitIO or GPIO component,

then there will be Typical Usage:

pastedImage_4.png

I also attached the Processor Expert user guide for you .

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信