Static library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Static library

2,541 Views
martindusek
Contributor V

Hello,

how to compile a static library in CodeWarrior for MCU Version: 10.2 Build Id:120126, that can be used in CrossWorks for ARM (GCC toolchain)?

 

Thanks

 

Martin


Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

2,065 Views
BlackNight
NXP Employee
NXP Employee

Hi Martin,

10.2 is pretty old, the actual version is 10.5. Things would be much easier for you if you would at least move to 10.4.

I used libraries with 10.3, and the following posts might help you to do the same thing with 10.2 (but not sure as I moved up to post 10.2 long time ago):

http://mcuoneclipse.com/2012/10/08/a-library-with-arm-gcc-and-eclipse/

Creating and using Libraries with ARM gcc and Eclipse | MCU on Eclipse

I hope this helps.

0 Kudos
Reply