Static library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Static library

2,470件の閲覧回数
martindusek
Contributor V

Hello,

how to compile a static library in CodeWarrior for MCU Version: 10.2 Build Id:120126, that can be used in CrossWorks for ARM (GCC toolchain)?

 

Thanks

 

Martin


ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,994件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Martin,

10.2 is pretty old, the actual version is 10.5. Things would be much easier for you if you would at least move to 10.4.

I used libraries with 10.3, and the following posts might help you to do the same thing with 10.2 (but not sure as I moved up to post 10.2 long time ago):

http://mcuoneclipse.com/2012/10/08/a-library-with-arm-gcc-and-eclipse/

Creating and using Libraries with ARM gcc and Eclipse | MCU on Eclipse

I hope this helps.

0 件の賞賛
返信