Standalone or cheaper CodeWarrior Flash Programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Standalone or cheaper CodeWarrior Flash Programmer

2,793 Views
tomsaluzzo
Contributor III

We are using CodeWarrior for PA in the Developer's Level. Is there a special CodeWarrior license that is cheaper than the development license that will just let us use the Flash programmer, or a standalone version of just the Flash programmer?

Labels (1)
0 Kudos
Reply
6 Replies

2,541 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Tom Saluzzo,

For the current CodeWarrior license information, please refer  to CodeWarrior Suite for Networked Applications|Freescale .

In addition, which processor does the customer use?

Thanks,

Yiping

0 Kudos
Reply

2,541 Views
tomsaluzzo
Contributor III

I ended up finding the answer through another path.

There is an Eclipse hosted CW for PA (v10.5) option within the basic suite.  This supports Flash programming for the T2080.  License is $395 for node locked, annual subscription. Part # CWA-BASIC-NL. Also have floating and perpetual licenses available.

You can see the options here:

http://www.freescale.com/tools/embedded-software-and-tools/software-development-tools/codewarrior-de...

2,541 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Tom Saluzzo,

CodeWarrior license for QorIQ is not sold separately to customers any more since July 2015. If customers want to use CodeWarrior, they have to purchase licenses for CodeWarrior Development Suites for Networked Application, which is a software packages including CodeWarrior, QCVS, Scenarios Tool, DDRv, Serdes Validation tool, etc. Please refer to the detailed license information from http://www.freescale.com/tools/embedded-software-and-tools/software-development-tools/codewarrior-de..., the customer needs to purchase "Developer Level" license at least.

It's better to contact Freescale local FAE to confirm whether there is new marketing policy for customers recently.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,541 Views
addiyi
NXP Employee
NXP Employee

I not sure this is what you are looking for. Basic license is for CodeWarrior for MCU and for CodeWarrior for PA Classic, but not for CodeWarrior for PA eclipse based. And only CodeWarrior for PA eclipse based provide support for your SoC.

Please contact your local FAE for more information.

Adrian

0 Kudos
Reply

2,541 Views
tomsaluzzo
Contributor III

Customer is using T2080.

0 Kudos
Reply

2,541 Views
addiyi
NXP Employee
NXP Employee

Standalone version for Flash Programmer is not available. For other types of CW license please contact a FAE.

Adrian

0 Kudos
Reply