Simulator Tool for Code warrior for Kinetic Family

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simulator Tool for Code warrior for Kinetic Family

Jump to solution
2,631 Views
utsavikalpesh
Contributor V

Hi,

 

I m working on code warrior 10.6 with mqx v4.0.

 

To see the output I need to load the Code into TWRK60D100M tower kit everytime.


So is there any tool for simulation purpose....??? to see the output of code without downloading the code in kit.


Labels (1)
0 Kudos
Reply
1 Solution
2,377 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Utsavi Kalpesh:

Unfortunately simulation is not supported for Kinetis MCUs in CodeWarrior or KDS and there is no tool or plugin for this purpose.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,378 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Utsavi Kalpesh:

Unfortunately simulation is not supported for Kinetis MCUs in CodeWarrior or KDS and there is no tool or plugin for this purpose.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,377 Views
utsavikalpesh
Contributor V

Hi Jorge,

Thnx for informing.

0 Kudos
Reply