Simulator Tool for Code warrior for Kinetic Family

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simulator Tool for Code warrior for Kinetic Family

ソリューションへジャンプ
2,665件の閲覧回数
utsavikalpesh
Contributor V

Hi,

 

I m working on code warrior 10.6 with mqx v4.0.

 

To see the output I need to load the Code into TWRK60D100M tower kit everytime.


So is there any tool for simulation purpose....??? to see the output of code without downloading the code in kit.


ラベル(1)
0 件の賞賛
返信
1 解決策
2,411件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Utsavi Kalpesh:

Unfortunately simulation is not supported for Kinetis MCUs in CodeWarrior or KDS and there is no tool or plugin for this purpose.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,412件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Utsavi Kalpesh:

Unfortunately simulation is not supported for Kinetis MCUs in CodeWarrior or KDS and there is no tool or plugin for this purpose.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,411件の閲覧回数
utsavikalpesh
Contributor V

Hi Jorge,

Thnx for informing.

0 件の賞賛
返信