Secure unsecure device under codewarrior ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure unsecure device under codewarrior ?

1,773 Views
kleckerspur
Contributor III

Hello,

 

How to secure unsecure MCF52259 or may be a different µC under CW 10.x and MQX 4.1 ?

 

thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,418 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello kleckerspur:

Did you manage to find this information?. In case you are still in doubt, the answers provided by Carlos Casillas and Juan Aguirre in the next thread will be useful for you:

Flash security, securing on MCF52259 (MCF5213) Coldfire

The security options are loaded from the flash configuration field at reset, and copied to CFMSEC register.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply