SPIMaster_LDD internal error?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPIMaster_LDD internal error?

2,094 次查看
leoo
Contributor I

Hi, I'm using CW 10.2 for MCU and added component SM2:SPIMaster_LDD to my project. I configure it. But, when I try to generate processor expert code, I got this error: "INTERNAL ERROR: at line 18: Unexpected status, please contact Freescale support. (file: Beans\IsPinRoutable.chg)    my_project SM2 Processor Expert Problem

I would like you to help me fix this problem.

Thanks in advance!

Regards,


L.

标签 (1)
标记 (5)
0 项奖励
回复
1 回复

1,948 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

CW for MCU v10.2 has been released at Q1 2012.

The last version is MCU v10.5.

It's difficult to say what is the problem.

Can you please try with last version ?

      just to know if the problem is solved or not.

else can you please provide us the project ?

++++++++++++++++++++

CodeWarrior for Microcontrollers v10.5 is the last version.

It integrates the development tools for the :

      ColdFire®, ColdFire+, DSC, Kinetis, Qorivva, PX, RS08, S08 and S12Z architectures

into a single product based on the Eclipse open development platform.

This version is running on Host platforms

      Microsoft® Windows XP 32/64-bit (Business)

      Windows Vista 32/64-bit (Business and Home Premium)

      Windows 7 32/64-bit (Professional and Home Premium)

      Windows 8 32/64-bit (Professional)

You can download an evaluation on the web site:

      http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10

++++++++++++++++++++

Regards

Pascal

0 项奖励
回复