SPI interrupt happens twice

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI interrupt happens twice

1,706 Views
mehdikarimibiuk
Contributor V

I have MK10DN512Z VLL10 with a bareboard project that has PE attached to it.

I have my SPI0 as my slave and sending data to it from outside.

 

1- I am not sure why the interrupt event "SlaveSPI0_OnBlockReceived" happens twice when I send data!

What I did, every time that I receive a 4 block data (each block is 16 bits), I see that the first time interrupt happens, and so I get the 4 block, but the second time that interrupt happens I don't have anything to pick and so it sends zeros only! But I only send 4 blocks from my master. I don't send 8 blocks at all.

Another thing I did in my interrupt event I flush the RX to make sure overflow is not a problem:

 

void SlaveSPI0_OnBlockReceived(LDD_TUserData *UserDataPtr)

{

  printf("==========ISR event: SPI0 receive a block=========\n");

  if ((IO_READ32(Rx0SPI0)) != 0)

  {

  print_RX_FIFO();

  inbuff = (IO_READ32(Rx0SPI0)<<16);

  inbuff |= IO_READ32(Rx1SPI0);

  extended_inbuff = (IO_READ32(Rx2SPI0)<<16);

  extended_inbuff |= IO_READ32(Rx3SPI0);

  }

  RX_FIFO_flush();

  TX_FIFO_flush();

  DataReceiveFlagSlave1 = TRUE;

}

 

 

and this is what I see in my shell:

 

==========ISR event: SPI0 receive a block========= (THIS IS FIRST TIME)

SR_SPI0 = 0x3344

RX0 = 0x1122    RX1 = 0x3344

RX2 = 0x5566    RX3 = 0x7788

==========ISR event: SPI0 receive a block========= (THIS IS SECOND TIME, HUH!!!)

 

 

2- I also looked into SPI0 Interrupt vector at address: 0xA8 and also the normal interrupt at address 0x84. I see that the values inside these vectors do not change, which is surprising to me!!! I expect these values change! Where can I look into what register or vector to see what is triggering the second interrupt?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,517 Views
Ray_V
Contributor V

The processor has only one handler for all SPI0 and one for all SPI1 interrupts.

There are several possible sources of SPI0 interrupt.

- End of Queue reached (EOQF)

- TX FIFO is not full (TFFF)

- Transfer of current frame complete (TCF)

- Attempt to transmit with an empty Transmit FIFO (TFUF)

- RX FIFO is not empty (RFDF)

- Frame received while Receive FIFO is full (RFOF)

 They are enabled by the SPI0_RSER register. You probably have two interrupts enabled (for example TCF and RFDF).

You need to check register SPI0_RSER to see which interrupts are enabled and register SPI0_SR to see which conditions have caused the interrupt.

Hope this helps

0 Kudos
Reply