S12DP512 RAM and Flash size checking

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12DP512 RAM and Flash size checking

1,806件の閲覧回数
monstor
Contributor II

There is 512KBytes flash size of S12DP512. How can I check the Ram and Flash usage this MCU?

 

Thanks for your helping.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,564件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

after a successfully project build, CW will generate a map file  in project "bin"  folder.

the map file details the flash/RAM usage.

the summary is also listed, for example:

Summary of section sizes per section type:

READ_ONLY (R):          91 (dec:      145)

READ_WRITE (R/W):      100 (dec:      256)

here,  READ_ONLY (R) is Flash usage.

READ_WRITE (R/W) is RAM usage.

can this help you?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信