Re: artifact name

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: artifact name

2,028 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Stefano,

 

Could you tell us which MCU and CodeWarrior version are you using?

 

Thanks in advance!

 

Best Regards,

Carlos Mendoza

Technical Support Engineer

Labels (1)
0 Kudos
Reply
1 Reply

1,832 Views
stefanomanca
Contributor III

Hi, I can't answer by web.I'm using CW 10.6 and kinetis kl15.Thank you.

-


Messaggio originale----

Da: "Carlos_Mendoza" <[email protected]>

Data: 30/05/2016 17.59

A: "stefano manca"<[email protected]>

Ogg: Re: - artifact name

a

body {

font-family: Helvetica, Arial, sans-serif;

-webkit-text-size-adjust: 100%;

}

h1, h2, h3, h4, h5, h6, p, hr {

-webkit-margin-before: 0;

-webkit-margin-after: 0;

-webkit-margin-start: 0;

-webkit-margin-end: 0;

}

.button td {

background-image: -moz-linear-gradient(top, #75B7E3 0%, #5498D6 50%, #408BD0 51%, #387AC8 100%) !important;

background-image: -webkit-gradient(linear, left top, left bottom, color-stop(0%,#75B7E3), color-stop(50%,#5498D6), color-stop(51%,#408BD0), color-stop(100%,#387AC8)) !important;

-webkit-box-shadow: inset 0 1px 0 #74b9de, 0 1px 3px rgba(0,0,0,.3) !important;

-moz-box-shadow: inset 0 1px 0 #74b9de, 0 1px 3px rgba(0,0,0,.3) !important;

}

-->

NXP Community

artifact name

reply from Carlos_Mendoza in CodeWarrior Development Tools - View the full discussion

Hi Stefano,

Could you tell us which MCU and CodeWarrior version are you using?

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in CodeWarrior Development Tools by email or at NXP Community

Following artifact name in these streams:

Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 Kudos
Reply