RTOS support for MK22FX512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTOS support for MK22FX512

2,586 Views
mayursavaj
Contributor III

Is there any RTOS support available for MK22FX512 controller? If yes than Please share docs and sample example code.

Thanks in Advance,

Mayur Savaj

0 Kudos
Reply
2 Replies

2,498 Views
ErichStyger
Specialist I

Hi @Mayur Savaj

I'm using FreeRTOS, and have examples on GitHub:

mcuoneclipse/Examples/MCUXpresso/K22FX512 at master · ErichStyger/mcuoneclipse · GitHub 

FreeRTOS is included in the NXP MCUXpresso SDK and the MCUXpresso IDE includes nice views and support for it.

I hope this helps,

Erich

2,498 Views
soledad
NXP Employee
NXP Employee

Hi,

I suggest you use FreeRTOS. You can download the SDK for the K22FX512 and add the FreeRTOS, after downloading it you will find some example codes that you can use as reference.

pastedImage_1.png

I hope this helps, have a nice day!

Regards

Soledad