Question Regarding CW QCVS 10.5.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question Regarding CW QCVS 10.5.1

1,896 Views
michayardeny
Contributor III

There is a problem when I load a valid rcw of t1042 

The problem said the follows: 


Custom value can be used only if "Ignore Constraints and non-Critical Errors" option is turned ON (HWA_CGA_M1_CLK_SEL [224-226]) c4 PBL/HWA_CGA_M1_CLK_SEL [224-226] Processor Expert Problem

I know there is an option to ignore it but i don't find it , can you help?

The version used is: 

Version: 10.5.1
Build Id:160128

Tags (2)
0 Kudos
Reply
1 Reply

1,761 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Micha Yardeny,

Please click "view menu" on the right of "Basic Advance" in "Component Inspector-PBL" panel, then select "Ignore Constraints and non-Critical Errors".

Please refer to the attachment.

Thanks,

Yiping

0 Kudos
Reply