QSCI baudrate setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QSCI baudrate setting

5,613件の閲覧回数
Ujwala_kontham
Contributor I

Iam using Serial LDD component in Code worrier 11.1 and setting the baud rate of 115200 in the configuration but in actual generated code it is setting the baud rate as 57600 i.e., 1 index less in baud rate table, this is same for all baud rate, can I get a solution for this to set it as required.

 

 

0 件の賞賛
返信
10 返答(返信)

5,567件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the SCI0 driving clock can be BUS_CLK or 2xBUS_CLK.
Pls check if you use BUS_CLK or 2xBUS_CLK by checking the SIM_PCR register.
This is from the RM of MC56F827xx.
 
xiangjun_rong_0-1709543325017.pngxiangjun_rong_0-1709543325017.png

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

5,565件の閲覧回数
Ujwala_kontham
Contributor I

yes in both the cases it is setting that same .

that means if we configure it for 115200 it setting baud rate of 57600

and if we configure it for 230400 it setting baud rate of 115200

0 件の賞賛
返信

5,550件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Okay, it appears that it is a bug of  Processor Expert, in the debug, pls read the QSCIx_RATE register, and tell us the BUS_CLK clock frequency you are using, then compute the baud rate of SCI based on the BUS_CLK or 2XBUS_CLK.

xiangjun_rong_0-1709606568473.pngxiangjun_rong_0-1709606568473.png

If baud rate does not match with the expected, it is a bug of PE.

Hope it can help you

BR'

XiangJun Rong

0 件の賞賛
返信

5,547件の閲覧回数
Ujwala_kontham
Contributor I

Iam using 30MHz of bus clock frequency and operating CPU in fast mode which intern sets core clock frequency and system clock frequency as 60MHz, and we debugged using both BUS_Clk and 2XBUS_Clck and got below values of QSCIx_RATE and QSCIx_CTRL3 registers respectively.
using BUS_CLk - 0104(RATE), 0000(CTRL3)
using 2XBUS_Clk - 0209(RATE), 0000(CTRL3)
and we also found that TimerInt_LDD component we are getting interrupt at double the time set in configuration that means if we configure it as 100us getting interrupt at 200us.

0 件の賞賛
返信

5,542件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If the BUS_CLK clock frequency is 30MHz, the baud rate will be:
case1:
using BUS_CLk - 0104(RATE),  baud rate=BUS_CLK/(16 *SBR)=30MHz(16*32.5)=57.7KHz instead of 115.2KHz
 
using 2XBUS_Clk - 0209(RATE),baud rate=2XBUS_CLK/(16 *SBR)=60MHz(16*65)=57.7KHz instead of 115.2KHz
 
Obviously, the code generated by PE has issue. Now and in the coming days, only SDK will be supported.
Sorry for the incorrect code.
BR
XiangJun Rong
0 件の賞賛
返信

5,539件の閲覧回数
Ujwala_kontham
Contributor I

can i get SDK for my controller (MC56F82746)?

0 件の賞賛
返信

5,525件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that MC56F82746 does not have tower board, so you have to select Processor as the following fig:

xiangjun_rong_0-1709692887828.pngxiangjun_rong_0-1709692887828.png

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

5,522件の閲覧回数
Ujwala_kontham
Contributor I

even after downloadind SDK of 2746 getting the project of 2748

 

 

0 件の賞賛
返信

5,576件の閲覧回数
Ujwala_kontham
Contributor I

Iam using MC56F82746 VLF controller

0 件の賞賛
返信

5,602件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Can you tell us which device are you using please?

0 件の賞賛
返信