QCVS DDR margin tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QCVS DDR margin tool

12,909 Views
OneNote
Contributor I

Hi

In our latest codewarriro QCVS, the margin page of DDR validation doesn't have Margin stage as scenarios, only has Diags margin stage. Why this happen? What's the cause?

Thanks.

 

0 Kudos
Reply
22 Replies

12,016 Views
yipingwang
NXP TechSupport
NXP TechSupport

What processor are you using now?

Which version QCVS tool are you using?

0 Kudos
Reply

12,014 Views
OneNote-0
Contributor I

Thanks, Yiping.

Processor: LX2160A

QCVS version: 4.23

0 Kudos
Reply

12,012 Views
yipingwang
NXP TechSupport
NXP TechSupport

Margin stage is removed since QCVS 4.23 2020.11 release.

Margin stage scenario is no longer available for LX2, but is should be available for the rest of devices.

If further information is needed, please feel free to let me know.

0 Kudos
Reply

12,009 Views
OneNote-0
Contributor I

Thanks.

Further question: how to test margin? use diag margin stage?

 

0 Kudos
Reply

12,004 Views
yipingwang
NXP TechSupport
NXP TechSupport

I just got confirmation from the development team.

Yes, you should use the diag margin stage.

 

0 Kudos
Reply

11,894 Views
OneNote
Contributor I

Thanks.

Now it's back to 4.22.

There is a new issue happen when run the margin test.

Log attached.

read margin test log.JPGread margin test log.JPG

0 Kudos
Reply

11,889 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please open CCS console on the right bottom of your task bar, type "log v", then connect to the target board again, the low level CCS log will be printed out.

Please send the CCS console log to me to do more investigation.

0 Kudos
Reply

11,884 Views
OneNote
Contributor I

ccs.JPGccs.JPG

 

Is this what you want? Thanks.

0 Kudos
Reply

11,882 Views
OneNote
Contributor I

CCS1.JPGCCS1.JPG

0 Kudos
Reply

11,858 Views
yipingwang
NXP TechSupport
NXP TechSupport

It failed at "reset_to_debug". If the RCW is valid, probably there is hardware design problem of the JTAG interface on your custom board.

0 Kudos
Reply

11,848 Views
OneNote
Contributor I

Measured the reset signals, when nRESET is low, PORESET_B also is low. And also found the HRESET_B is low and keep low always.Is it a clue?

0 Kudos
Reply

11,836 Views
yipingwang
NXP TechSupport
NXP TechSupport

Would you please refer to "3.2 Working with bareboard application" in the attached document to create a board board project and run it on your target board.

Please click "Target Connections->LX2160A_RDB(1)->Edit->Target Initialization File", 

please modify "USE_SAFE_RCW = False" to "USE_SAFE_RCW = True".

Then connect to the target board, and send CCS console log to me, I just want to check whether the core can be stopped.

0 Kudos
Reply

11,826 Views
OneNote
Contributor I

Print3.JPGPrint3.JPG

0 Kudos
Reply

11,824 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please modify "USE_SAFE_RCW = False" to "USE_SAFE_RCW = True" in CW initialization file and save the configuration.

0 Kudos
Reply

11,834 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please also try the following commands in CCS console.

delete all

config cc cwtap:<ip>

ccs::config_chain {lx2160a dap}

display ::ccs::get_config_chain

::ccs::stop_multi_core {21}

::ccs::reset_to_debug

0 Kudos
Reply

11,830 Views
OneNote
Contributor I

Print1.JPGPrint1.JPGPrint0.JPGPrint0.JPG

0 Kudos
Reply

11,828 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please try to run a bareboard application with hard-coded RCW as I mentioned in my previous post.

0 Kudos
Reply

11,823 Views
OneNote
Contributor I

Print4.JPGPrint4.JPG

0 Kudos
Reply

11,817 Views
yipingwang
NXP TechSupport
NXP TechSupport

As I mentioned previously, please modify "USE_SAFE_RCW = False" to "USE_SAFE_RCW = True" in CW initialization file and save the configuration, then run the bareboard application.

0 Kudos
Reply

11,852 Views
yipingwang
NXP TechSupport
NXP TechSupport

Is it possible to provide your JTAG design schematics for the custom board?

0 Kudos
Reply