Program NTM88 with USBDM in CodeWarior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Program NTM88 with USBDM in CodeWarior

2,928 次查看
alesgabersek
Contributor I

Hello,

I tried to compile and run demo for NTM88 in CodeWarior v11.1 using USBDM v4.12 and I have connection problem. As stated in instructions I have also installed patch "com.freescale.mcu11_1.HCS08_NTM88_LIB.win.sp.v1.0.2.zip".

When I try to run program from CodeWarior, it stops at 76% and reports one of following errors:

-"Error launching New_configuration"

-"USBDM - Target connection failure ... Retry connection ... yes/no"

Diagnostics report is in attachment.

I also tried using "HCS08 Programming" application it detects chip as "FXTH87" and I could also compare demo hex with program on chip (Verify flash) which naturaly reports difference.

I also tried changing settings of USDM, but without success.

Regards, Ales

0 项奖励
回复
2 回复数

2,519 次查看
nguyenhuy5997
Contributor I

have you found the solotion, i meet the same problem

0 项奖励
回复

2,922 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ales,

 

We are not using USBDM so I cannot give feedback on it.

We recommend using the P&E Micro USB Multilink Universal:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/mac57dxxx/universal-multi...

 

Best regards,

Tomas

 

 

0 项奖励
回复