Processor Expert USBDIV

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert USBDIV

1,164件の閲覧回数
Mike_d
Contributor IV

I'm trying to run the Core of a K64 @120MHz but I don't see how to modify USBDIV to get the 48MHz it needs.

ラベル(1)
0 件の賞賛
返信
1 返信

1,066件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Michael,

this is how I set it to 120 MHz:

FRDM-K64F at Maximum Speed of 120 MHz | MCU on Eclipse

And here is how I use it for USB:

USB CDC with the FRDM-K64F, finally! | MCU on Eclipse

Settings:

CPU:

USB:

pastedImage_2.png

I hope this helps,

Erich

0 件の賞賛
返信