Processor Expert QuadratureDecoder component on KV10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert QuadratureDecoder component on KV10

1,716件の閲覧回数
jaydcarlson
Contributor III

I'd like to try out the new KV10 for a sensored BLDC design. The motor I'm using has a quadrature encoder (in addition to the Hall effect sensors), so I'd like to use the KV10's quadrature decoder -- however, the QuadratureDecoder module in Processor Expert doesn't appear to support the KV10. Is there an easy way of getting the module to work? Or hacking the timer module to function as a quadrature decoder? I know I can do it in software, but if the peripheral is there, why not use it?

 

Thanks!

ラベル(1)
0 件の賞賛
返信
1 返信

1,498件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jay,

please refer thread here:

Re: In the codewarrior did not find the Quadrature Decoder

i think it can be useful.

================================

this answer is for you. if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 件の賞賛
返信