Problems flashing mc12xe with code warrior.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems flashing mc12xe with code warrior.

ソリューションへジャンプ
1,773件の閲覧回数
kobrons
Contributor I

I'm using a devkit-s12xe, connected it to a power source and a Laptop via usb.

I'm not able to flash the program on the chip when using one of the included example projects or a fresh one.

The Error Message says: "Error while loading diagnostics algorithm to target system. The chip may be secured, or the derivative selected may be wrong"

I've checked the derivative to make shure it's the one on the board and when trying to unsecure the flash I get the following error message: "Derivative could NOT be unsecured!!!! The unsercure command file might be missing or disabled. Make sure the command file defined in the Unsecure panel of the Command File dialog contains the correct commands to unsecure the current connected derivative and board oscillator frequency."

I've checked the unsecure file but couldn't find any errors in it.

Is there anything else I can do?

Thanks

0 件の賞賛
返信
1 解決策
1,645件の閲覧回数
kobrons
Contributor I

never mind. I found the Problem.

The recommendet CodeWarrior Version on the Productpage didn't work for me. I downloadet CW 5.2 now it works.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,646件の閲覧回数
kobrons
Contributor I

never mind. I found the Problem.

The recommendet CodeWarrior Version on the Productpage didn't work for me. I downloadet CW 5.2 now it works.

0 件の賞賛
返信