Problems!FreeMASTER communication through CAN!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems!FreeMASTER communication through CAN!

4,028件の閲覧回数
pengjianxin
Contributor II

hello:

       i intergrated the freemaster codes into my application code,and download the S19 file into the evaluation bord.

       the communication configuration is :

      (1)short-inter mode;

      (2) the FMSTR_Poll() is in for(;;),FMSTR_Isr() is in can receive interrupt function; FMSTR_Init();

      (3)FlexCAN,  SPC56**

Then, the result of “Test Connection”:

                  " target is alive (responded to ping)"

 

           the standard frame 0x7aa send and the response is received,but in the next step i click the button " STOP " to start communication,the results is below:

           " Can not detec the board information! the  communication  will paused. Error code: 0x858e0003

 

I have several questions:

(1) Freemater through CAN, the protocol of communication is XCP/CCP? because i do not find the protocol in the specification,please confirm the information。

(2) without can protocol,how can i fix the problem?

                   looking forward to your  response,My E@mal is" [email protected] ", thank you.

タグ(2)
0 件の賞賛
返信
1 返信

3,700件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello,

To make the debugging of this issue a bit simpler I'd recommend you to start with polling mode first since the complexity of the interrupts is not involved.

#define FMSTR_POLL_DRIVEN 1

Please make sure CAN ID on the target matches with embedded side (FMSTR_CAN_CMDID, FMSTR_CAN_RESPID - freemaster_defcfg.h). Default value is 0x7aa.

Also you can try to increase the response timeout:

pastedImage_2.png

FreeMASTER does not use XCP/CPP protocol but its own protocol (see fremaster_protocol.c/freemaster_protocol.h)

Hope it helps.

Stan

0 件の賞賛
返信