Problem recover T4240RDB board using CodeWarrior Flash Programmer v10.4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem recover T4240RDB board using CodeWarrior Flash Programmer v10.4

跳至解决方案
11,675 次查看
paololago
Contributor I

Hi,

I'm trying to use the Codewarrior USB TAP and the flash programmer to flash a u-boot binary image to my t4240rdb board, but I do not know which connection I have to choose in the Flash File to Target dialog:

19578_19578.pngFlash File to Target.png

can you help me?

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
10,737 次查看
lunminliang
NXP Employee
NXP Employee

Hi,

May be you can try to run the Bareboard project with RCW override to see if connection OK. Use the T4240RDB_init_sram.tcl to be initialization file and choose CodeWarrior USB TAP to be the connection type(Both when you create the project or change the settings after creating are OK). Specify T4240RDB_RCW...-rev2.0.txt or T4240RDB_RCW...-rev1.0 in the JTAG file configuration panel, according to chip version on the board.


Regards


在原帖中查看解决方案

0 项奖励
回复
20 回复数
10,737 次查看
addiyi
NXP Employee
NXP Employee
10,737 次查看
paololago
Contributor I

Hi Adrian,

thanks for the reply.

I have already followed that Application Note without success.

In particular, after configuring a flash device as described in Section 3, the execute button is not green. This is because the debugger is not running and I do not know how to configure it.


Paolo

0 项奖励
回复
10,734 次查看
addiyi
NXP Employee
NXP Employee

Hi Paolo,

You have 2 possibilities. One is to enter in debug and then run the target task and the second is to right click on target task and Change Run Configuration from Active Debug Context to a run configuration you want to use.

Adrian

10,735 次查看
paololago
Contributor I

Ok , I'm trying to create a run configuration and the following dialog appears:

  run_conf.png

I suppose that I have to configure a connection in the target settings box (am I wrong?)

Then, after clicking the "New" button, the following dialog appears:
run_conf.png

Here there are several system types, but not my board ( the t4240rdb ).

The problem is that I do not know how to configure a debug or a run configuration for simply flash a file on my board and I did not find any guide explaining this. :smileysad:

0 项奖励
回复
10,735 次查看
addiyi
NXP Employee
NXP Employee

Again you have two possibilities :smileyhappy:. First one is to create a bareboard project using Wizard, and select Download/Attach as launch. Then select this debug config in "Change Run Configuration".


Second from New Connection you should select Hardware or Simulator Connection, provide a name and description. As Target go to New - > Hardware or Simulator Connection. Then at Target type expand eppc and select T4240. In Initialization tab: Select the core(s), add Initialize target file. In Memory tab add the memory file. Those files can be found in CW_PA_v10.4.0\PA\PA_Support\Initialization_Files\. Then select this configuration in "Change Run Configuration".

0 项奖励
回复
10,735 次查看
paololago
Contributor I

Ok, I created a bareboard project and I added the memory file "T4240RDB.mem" and the initialize target file "T4240RDB_init_sram.tcl" (as suggested by the Application Note you sent to me). Then I clicked execute, but unfortunately I get the following error message below:

fl::target -lc "rec-core00_RAM_T4240_Download"

fl::target -b 0x0 0x180000

fl::target -v off -l off

cmdwin::fl::device -d "S29GL01GP" -o "64Mx16x1" -a 0xe8000000 0xefffffff

cmdwin::fl::image -f "C:\\Users\\Paolo\\Documents\\u-boot-T4240RDB-2014.07+fslgit-r0.bin" -t "Auto Detect" -re on -r 0xeff40000 0xefffffff -oe on -o 0xeff40000

cmdwin::fl::write

Beginning Operation ...

-------------------------

Using restricted address range 0xEFF40000 to 0xEFFFFFFF

Programming file C:\Users\Paolo\Documents\u-boot-T4240RDB-2014.07+fslgit-r0.bin

Auto-detection is successful.

  File is of type Binary/Raw Format.

Performing target initialization ...

Error:  Connect Failed.

Failed to reset the target

[CCS last error: T4240: Scan timeout ](CCSProtocolPlugin)

Error: Connect Failed.

Thank you in advance for your support Adrian.

Paolo

0 项奖励
回复
10,735 次查看
addiyi
NXP Employee
NXP Employee

2.PNG.pngMake sure your Add Program Action looks like in the screenshot.

0 项奖励
回复
10,735 次查看
paololago
Contributor I

Yes my Program/Verify window looks exactly like the your one.

Let me summarize what I did till now:

- as you said, I created a bareboard project, and I selected Download/Attach as launch

- then, in the "Change Run Configuration" I choosed this debug configuration

- when I execute the Target Task I get this error message in the console: "Core not responding"

Error:  Connect Failed.

Failed to reset the target

[CCS last error: T4240: Core not responding ](CCSProtocolPlugin)

Error: Connect Failed.

Paolo

0 项奖励
回复
10,735 次查看
addiyi
NXP Employee
NXP Employee

"Core not responding error" is not ok. It could indicate a hardware issue. To check this please go to CW_PA_v10.4.0\PA\ccs\bin\, open ccs.exe and enter the commands:

(bin) 175 % delete all

(bin) 176 % config cc cwtap

(bin) 177 % show cc

(bin) 178 % ccs::config_chain t4amp

(bin) 179 % ccs::reset_to_debug

If you get "Core not responding error", it is very possible to be a hardware issue with the board.

Adrian

0 项奖励
回复
10,735 次查看
paololago
Contributor I

The "show cc" command gives me this error message: "0: CC config string is invalid"

0 项奖励
回复
10,735 次查看
addiyi
NXP Employee
NXP Employee

Do you use a CodeWarrior TAP or CodeWarrior USB TAP? If you use first tap it is over usb or ethernet?

Adrian

0 项奖励
回复
10,735 次查看
paololago
Contributor I

I'm using the CodeWarrior USB TAP, there is no ethernet socket.

Paolo

0 项奖励
回复
10,735 次查看
addiyi
NXP Employee
NXP Employee

Ok. Then use:

(bin) 175 % delete all

(bin) 176 % config cc utap

(bin) 177 % show cc

(bin) 178 % ccs::config_chain t4amp

(bin) 179 % ccs::reset_to_debug

Adrian

0 项奖励
回复
10,737 次查看
paololago
Contributor I

I always get the same error: CC config string is invalid

cc.png

0 项奖励
回复
10,737 次查看
addiyi
NXP Employee
NXP Employee

Than, thy the following commands:

findcc utaps - this will display all available utap connection

findcc cwtaps - this will display all available cwtap connection

Adrian

0 项奖励
回复
10,737 次查看
paololago
Contributor I

Ok the previous command finally worked, I get Core not responding:

cc.png 

0 项奖励
回复
10,737 次查看
addiyi
NXP Employee
NXP Employee

Before we say this is a hardware issue, please refer to T4240RDB_aeabi_README.txt and make sure the switches are set according with the CPU revision.

Adrian

0 项奖励
回复
10,737 次查看
paololago
Contributor I

All switches are set correctly as reported in T4240RDB_aeabi_README.txt

Paolo

0 项奖励
回复
10,737 次查看
lunminliang
NXP Employee
NXP Employee

Hi,

May be you can try to run the Bareboard project with RCW override to see if connection OK. Use the T4240RDB_init_sram.tcl to be initialization file and choose CodeWarrior USB TAP to be the connection type(Both when you create the project or change the settings after creating are OK). Specify T4240RDB_RCW...-rev2.0.txt or T4240RDB_RCW...-rev1.0 in the JTAG file configuration panel, according to chip version on the board.


Regards


0 项奖励
回复
10,734 次查看
paololago
Contributor I

Hi,

With the RCW override the flashing process works correctly.

Now I can try to recover my board.

Thank you

Paolo

0 项奖励
回复